Keysight VISA.NET Help
WriteLineList(SByte[]) Method



The array of signed bytes to be added to the formatted I/O write buffer.
Converts each of the signed bytes in the specified array to an ASCII string and appends them, separated by commas, to the formatted I/O write buffer. Appends a newline (0xA) to the formatted I/O write buffer, flushes the buffer, and sends an END with the buffer if required.
Syntax
'Declaration
 
Overloads Sub WriteLineList( _
   ByVal data() As SByte _
) 
'Usage
 
Dim instance As IMessageBasedFormattedIO
Dim data() As SByte
 
instance.WriteLineList(data)
void WriteLineList( 
   sbyte[] data
)
void WriteLineList( 
   array<sbyte>^ data
) 

Parameters

data
The array of signed bytes to be added to the formatted I/O write buffer.
Requirements

Current with Keysight IO Libraries Suite 18

See Also

 

 


© Keysight Technologies 2015-2025